Power on the tower
with a boost from the ground
1
© 2018 CommScope, Inc. All rights reserved. All trademarks identified by ® or ™ are registered trademarks or trademarks, respectively, of CommScope, Inc. General Electric and the GE logo are registered trademarks of General Electric Company used with permission. MM-109562.2-OL (01/18)
Sources: (1) Infomine.com, November 13, 2017
Built for CommScope by the power experts at General Electric.
Hover over boxes for more
Extends RF battery uptime by up to 50%
Quadruples allowable cable length
Standardizes the installation process for all RRU power levels and cable lengths
Reduces tower loading by using smaller cables
®
The industry's first intelligent, plug-and-play DC power supply
Enter PowerShift
Increased power means more greenhouose gas emissions
The cost of energy continues to climb
Higher wattage RRUs currently require larger diameter power cables or additional cable runs.
That means more
power has to travel
up the cables.
1000-
1500W
500-
750W
100-
300W
2020-2030
2010
2001
As subscriber wireless usage increases, operators are moving to higher wattage RRUs.
Amplifiers and radio equipment account for more than 60% of the power consumed at the top of the cell site.
60%
4G/LTE
accelerated the use of a new cell site architecture that placed certain radio functions at the top of the tower for the very first time.
Remote Radio Units (RRU) at the top require power from the ground via power cables.
World price of copper
$ Per Ton
The cost of copper has risen 46% over the past year alone. This adds:
An increased chance of theft
More tower weight and wind loads
More expense to power cabling